This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
"This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU, with a change in range name going from Spacial SF to PanelSeT SFN. This version as well, provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view on the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased references"
In exposed environments, particular attention must be paid to the choice of enclosures. Stainless steel is the solution to resist aggression in exposed environments. This guide will help the reader to select the optimum stainless-steel enclosure accordingly.
Environmental disclosure
UE_Spacial SF, Steel floor-standing enclosure
English
2024-04-15
CAE
Spacial SM CAE package for EPLAN
SILENT
2024-04-15
Spacial SM CAE package for EPLAN
This package contains 2D and 3D macros for ePlan, related to SM enclosures and their accessories
Declaration of conformity
NSYTVR14 China RoHS Declaration
English
2024-04-02
NSYTVR14 China RoHS Declaration
Set of 2 heavy duty vertical rails for fixing of chassis and cross rails-1400 mm
NSYTVR14 EU RoHS Declaration
English
2024-04-02
NSYTVR14 EU RoHS Declaration
Set of 2 heavy duty vertical rails for fixing of chassis and cross rails-1400 mm
NSYTVR14 REACh Declaration
English
2024-04-02
NSYTVR14 REACh Declaration
Set of 2 heavy duty vertical rails for fixing of chassis and cross rails-1400 mm
Instruction sheet
Heavy duty vertical rails instruction Seet
SILENT
2024-04-15
CAD
Spacial SM - NSYTVR14 - 2 heavy duty vert.rails 1400