Auch bei Dunkelheit immer den Durchblick behalten.
Katalog
DIY catalogue fixing & tool for electricians
English
2024-06-15
DIY catalogue fixing & tool for electricians
All the small Equipment for the Professional and the handyman who need quality devices to accompany him in the electrical work.
installation materials
English
2024-06-15
installation materials
all the small devises needed to create an electrical installation. Junction , flush or surface mounted boxes, electrical conduits, cable reels, test meters, work lamps, electrical tapes, grommets, fixings, screws etc.
Merten Katalog
German
2024-06-15
Merten Katalog
Der Merten Katalog mit seinem Preisverzeichnis hilft dabei Produkte schneller zu finden, diese einfacher zu vergleichen und für eine Bestellung auszuwählen.
Technische Zeichnung
IMT47222-Energy-Label
English
2024-03-20
Gebrauchsanleitung
Mureva Lights - Floodlight - 150W to 300W - User Manual
English
2024-06-18
Mureva Lights - Floodlight - 150W to 300W - User Manual
The LED floodlight is powered by LED technology and offers better energy efficiency, superior lighting performance, and a longer lifetime. It is suitable to install in all weather conditions and is well suited for commercial and residential lighting applications. The floodlight is spray-protected and does not require any maintenance, such as, for example, replacement of the LED light sources. It has a non-dimmable light source.