This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
Instruction sheet
4000 A connection plate 10 mm Horizinral busbar - Vertical flat
SILENT
2024-01-02
Connection for 120 mm Hz busbars - Instruction Sheet