This protocol document provides setup instructions for using DLMS/COSEM with PowerLogic ION8650 (firmware v406 and later), ION7400 (firmware v1.4.1 and later) and ION8800 (firmware v350 and later) meters.
This document explains how to configure and operate ION9000 meters.
Upgrade meter firmware to v2.2.1
English
2024-06-15
Upgrade meter firmware to v2.2.1
This document describes the process to upgrade PowerLogic™ ION9000, PM8000 or ION7400 series meters to the latest firmware version. It also contains information about upgrading analog I/O option module firmware.
Upgrade PM89RD96 display firmware to v4.0.15
English
2024-06-15
Upgrade PM89RD96 display firmware to v4.0.15
This document describes the process to upgrade RD96 display firmware to the latest version for use with PowerLogic™ ION9000, PM8000 or ION7400 series meters.
What’s new in ION9000 series meter firmware v2.1.0
English
2024-05-15
What’s new in ION9000 series meter firmware v2.1.0
ION9000 firmware version 2.1.0 updates: 0-20 mA Analog I/O option module support, UPG to UPX firmware upgrade enhancement
Firmware
ION9000 v3.0.0 Firmware and Associated Files
English
2024-06-15
ION9000 v3.0.0 Firmware and Associated Files
'This ZIP file contains the files to upgrade the PowerLogic™ ION9000 series meter to firmware v3.0.0 (V003.000.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the Upgrading Meter Firmware to v3.0.0 document for important information on performing this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the ION9000_V003.000.000+599.zip file.Name: ION9000_V003.000.000+599.zipSHA256: 9615CA7795864FDC180C17139DFEBB3F9A3A7ACAFFF28BFB2045DBA8C5AEE357
ION9000 v4.0.0 Firmware and Associated Files
English
2024-06-15
ION9000 v4.0.0 Firmware and Associated Files
This ZIP file contains the files to upgrade the PowerLogic™ ION9000 series meter to firmware v4.0.0 (V004.000.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the upgrade section of the User Manual to perform this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the file. Name: ION9000_V004.000.000+200.zip Size: 43634681 bytes (41 MiB) SHA256: B71F0493170B8D23E50053FFC07DF096480BDA63CAC70AAF072DACF76CA64391
METSEPM89M0024 Analog I/O Module V001.002.000 firmware
English
2024-05-15
METSEPM89M0024 Analog I/O Module V001.002.000 firmware
The 1.2.0 (V001.002.000) firmware for the METSEPM89M0024 Analog I/O Module adds 0-20 mA support when used with PM8000, ION7400, or ION9000 meter firmware 2.1.0 (V002.001.000) or higher. SHA256 File signatures:77855de93e70ed9b25be9568b64eaa333c56ead286624323fbc04073cdb5626a *METSEPM89M0024_AIO_V001.002.000_Release.s19
PowerLogic METSERD192 Display OS Package Firmware version 4.0.5 - supports v2.0.0 meter firmware
English
2024-04-15
PowerLogic METSERD192 Display OS Package Firmware version 4.0.5 - supports v2.0.0 meter firmware
OS Package version 4.0.5 is the initial release for the METSERD192 remote display. It supports meter firmware version 2.0.0 for the PowerLogic™ ION9000 series meter.SHA256 File signatures:e4f192cac9b01f1ab24bde979d6fba88b47a3915358cc4b13051a7fa39e46ff6 *rmdupg_rd192_004.000.005.bin
PowerLogic PM89RD96 Display OS Package Firmware version 4.0.0 - supports v2.0.0 meter firmware
English
2024-06-15
PowerLogic PM89RD96 Display OS Package Firmware version 4.0.0 - supports v2.0.0 meter firmware
This is OS Package version 4.0.0 for the METSEPM89RD96 remote display. It supports meter firmware version 2.0.0, including the PowerLogic™ ION9000 series.See the Power Meter user manual for display firmware upgrade instructions.Note: This remote display OS Package is not compatible with PM8000 & ION7400 meters running firmware versions 1.4.x and older.SHA256 File signatures:8b0aaa760d1e705b7528ee3941e381c00cab3adc524b460a9fd04acf54a0ef37 *rmdupg_rd96_004.000.000.bin
Katalog
PowerLogic – Energiemanagement und Netzmesstechnik
German
2024-06-15
PowerLogic – Energiemanagement und Netzmesstechnik
Produkte und Systemlösungen zur Optimierung von Energiekosten, Netzqualität und Anlagenverfügbarkeit
Konformitätserklärung
UK Declaration of Conformity
English
2024-06-15
UK Declaration of Conformity
UK Declaration of Conformity for the ION9000 series meter
Entsorgungsinformation
PowerLogic ION9000 meter, Circularity Profile, End of Life Instructions