Instructions on how to install, configure, use, and maintain PowerLogic PM8000 series devices.
PowerLogic Серия PM8000 Руководство пользователя
Russian
2024-06-15
Upgrade meter firmware to v2.2.1
English
2024-06-15
Upgrade meter firmware to v2.2.1
This document describes the process to upgrade PowerLogic™ ION9000, PM8000 or ION7400 series meters to the latest firmware version. It also contains information about upgrading analog I/O option module firmware.
Upgrade PM89RD96 display firmware to v4.0.15
English
2024-06-15
Upgrade PM89RD96 display firmware to v4.0.15
This document describes the process to upgrade RD96 display firmware to the latest version for use with PowerLogic™ ION9000, PM8000 or ION7400 series meters.
What’s new in PM8000 series firmware v1.4.1
English
2024-06-15
What’s new in PM8000 series firmware v1.4.1
Firmware version v1.4.1 for the PM8000 series meter adds security enhancements, new communications functionality, increased onboard log storage capacity, a webpage waveform viewer and other improvements.
Software - Release
What's new in PowerLogic PM8000 series meter firmware v4.5.0
English
2024-06-15
What's new in PowerLogic PM8000 series meter firmware v4.5.0
Summary of the new features included in firmware version 4.5.0
Other technical guide
PowerLogic PM8000 Technical Datasheet
English
2024-06-15
Firmware
METSEPM89M0024 Analog I/O Module V001.002.000 firmware
English
2024-05-15
METSEPM89M0024 Analog I/O Module V001.002.000 firmware
The 1.2.0 (V001.002.000) firmware for the METSEPM89M0024 Analog I/O Module adds 0-20 mA support when used with PM8000, ION7400, or ION9000 meter firmware 2.1.0 (V002.001.000) or higher. SHA256 File signatures:77855de93e70ed9b25be9568b64eaa333c56ead286624323fbc04073cdb5626a *METSEPM89M0024_AIO_V001.002.000_Release.s19
PM8000 v3.1.0 Firmware and Associated Files
English
2024-06-15
PM8000 v3.1.0 Firmware and Associated Files
'This ZIP file contains the files to upgrade the PowerLogic™ PM8000 series meter to firmware v3.1.0 (V003.001.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the upgrade section of the User Manual to perform this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the file. Name: PM8000_V003.001.000+626.zip SHA256: 073C0192EE8A0B833F273AB7D65E7E51AD1C813590CE5CB56D859394F5A8EC6A
PowerLogic PM89RD96 Display OS Package Firmware version 4.0.0 - supports v2.0.0 meter firmware
English
2024-06-15
PowerLogic PM89RD96 Display OS Package Firmware version 4.0.0 - supports v2.0.0 meter firmware
This is OS Package version 4.0.0 for the METSEPM89RD96 remote display. It supports meter firmware version 2.0.0, including the PowerLogic™ ION9000 series.See the Power Meter user manual for display firmware upgrade instructions.Note: This remote display OS Package is not compatible with PM8000 & ION7400 meters running firmware versions 1.4.x and older.SHA256 File signatures:8b0aaa760d1e705b7528ee3941e381c00cab3adc524b460a9fd04acf54a0ef37 *rmdupg_rd96_004.000.000.bin