This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
"This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU, with a change in range name going from Spacial SF to PanelSeT SFN. This version as well, provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view on the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased references"
CAE
PanelSeT SFN complete range CAE package for EPLAN
SILENT
2024-04-15
PanelSeT SFN_NSYSPS4200_CAE package for EPLAN
English
2024-04-15
Környezetvédelmi közzététel
UE_Spacial SF, Steel floor-standing enclosure
English
2024-04-15
Megfelelőségi nyilatkozat
NSYSPS4200 EU RoHS nyilatkozat
Hungarian
2024-04-25
NSYSPS4200 EU RoHS nyilatkozat
4 oldalsó lábazati elem (400*200)
NSYSPS4200 Kínai RoHS nyilatkozat
Hungarian
2024-04-25
NSYSPS4200 Kínai RoHS nyilatkozat
4 oldalsó lábazati elem (400*200)
NSYSPS4200 REACh nyilatkozat
Hungarian
2024-04-25
NSYSPS4200 REACh nyilatkozat
4 oldalsó lábazati elem (400*200)
CAD
Spacial SM - 4 Plinth side panels 200x400 - 3D CAD