This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
In exposed environments, particular attention must be paid to the choice of enclosures. Stainless steel is the solution to resist aggression in exposed environments. This guide will help the reader to select the optimum stainless-steel enclosure accordingly.
Finden Sie in diesem Gesamtkatalog unser Angebot an Gehäuse- und Schranksystem-Baureihen. Spacial bietet Schaltschränke und Gehäuse aus Metall. Thalassa ist unsere Baureihe von Isolierschränken. ClimaSys sorgt für eine effiziente Termperaturregelung innerhalb Ihres Schaltschranks.
Produktumweltprofil
Spacial SMX - Stainless steel
English
2024-07-15
Spacial SMX - Stainless steel
PEP for stainless steel enclosures
Gebrauchsanleitung
Instruction shhet for staniless steel SFX-SMX plinths