The Installation Manual contains a device description, safety instructions, a description of the display, and the other information that you need to install the device.
TCSEFEA23F3F22 Tofino Firewall - Connexium, User Manual
English
2024-06-15
TCSEFEA23F3F22 Tofino Firewall - Connexium, User Manual
ConneXium Tofino Firewall: Referred to in this manual as the Tofino
Security Appliance or Tofino SA. These industrially hardened devices are
installed in front of individual and/or clusters of Human Machine Interfaces
(HMI), Distributed Control Systems (DCS), Programmable Logic
Controllers (PLC), or Remote Terminal Units (RTU) control devices that
require protection.
Das Dokument „Installations-Handbuch“ enthält eine Gerätebeschreibung,
Sicherheitshinweise, Anzeigebeschreibung und weitere Informationen, die
Sie zur Installation des Gerätes benötigen, bevor Sie mit der Konfiguration
des Gerätes beginnen.
TCSEFEA23F3F22 Tofino Firewall, Manual de instalación
Spanish
2024-04-15
TCSEFEA23F3F22 Tofino Firewall, Manuel d''installation