ATV212 Quick Start Annex (SCCR and Branch Circuit Protection)
English
2024-06-15
ATV212 Quick Start Annex (SCCR and Branch Circuit Protection)
Short Circuit Current Ratings (SCCR) and branch circuit protection Recommended fuse ratings for UL and CSA requirements. Components for use together in accordance with standard UL508C
How to configure ATV212 for a Fan application?
Example of speed regulation or Flow regulation according to a reference
Parameters changed:
- F113 between PID to Speed
- F201 to F204 as process reference (here the "flow")
- F210 to F213 for motor speed, motor rated voltage and frequency
- F360 enabling PID