This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
This new version of the document takes into account the launch of the new offers. It also takes into account the change in range name from all Spacial offer to PanelSeT and all Thalassa TBS/TBP to PanelSeT TBS/TBP.
Offer Marketing Illustration
Spacial CRN - Benefits - Marketing illustration
English
2024-06-20
Certifikat
DoC
Russian
2024-06-19
UL Certificate of SPACIAL CRNG enclosures
SILENT
2024-06-20
ЕАЭС_N_RU_Д-FR.PA01.B.80899_20
Russian
2024-06-19
Uporabniški priročnik
Spacial CRN - Changes to the largest enclosure (English)
Spacial CRN - Changes to the largest enclosure (English)
In 2023 the largest enclosures in the spacial CRN range will be undergoing a slight change. This document explains all these changes and puts forward all the information that might be needed to adapt panel assembling and fitting processes.
Navodila za uporabo
CRNG assembly instructions
English,French
2024-06-20
Izjava o skladnosti
NSYCRNG1210300D Dobaviteljeva izjava o skladnosti EU
Slovenian
2024-06-28
NSYCRNG1210300D Dobaviteljeva izjava o skladnosti EU
2 navadnih vrat Spacial CRNG brez mont. pl. V1200xŠ1000xG300 IP55 IK10 RAL7035
NSYCRNG1210300D Dobaviteljeva izjava o skladnosti Kitajske
Slovenian
2024-06-28
NSYCRNG1210300D Dobaviteljeva izjava o skladnosti Kitajske
2 navadnih vrat Spacial CRNG brez mont. pl. V1200xŠ1000xG300 IP55 IK10 RAL7035
NSYCRNG1210300D Uredba REACH
Slovenian
2024-06-28
NSYCRNG1210300D Uredba REACH
2 navadnih vrat Spacial CRNG brez mont. pl. V1200xŠ1000xG300 IP55 IK10 RAL7035
CAD
DXF Drawings for Enclosure CRN 1200x1000x300
SILENT
2024-06-20
Spacial CRN - CRNG 2 plain doors without mounting plate H1200xW1000xD300 - 3D CAD