This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
This new version of the document takes into account the launch of the new offers. It also takes into account the change in range name from all Spacial offer to PanelSeT and all Thalassa TBS/TBP to PanelSeT TBS/TBP.
Universal Enclosures - Quick Selection Guide without CRN (2024 EN)
English
2024-06-19
Universal Enclosures - Quick Selection Guide without CRN (2024 EN)
This new version of the document takes into account the launch of the new offers. It also takes into account the change in range name from all Spacial offer to PanelSeT and all Thalassa TBS/TBP to PanelSeT TBS/TBP.
Razkritje informacij v zvezi z okoljem
UE_Spacial SF, Steel floor-standing enclosure
English
2024-06-15
Izjava o skladnosti
NSYSPS3200 Dobaviteljeva izjava o skladnosti EU
Slovenian
2024-06-19
NSYSPS3200 Dobaviteljeva izjava o skladnosti EU
Stranska plošča podnožja Spacial SM - 200 x 300 mm
NSYSPS3200 Dobaviteljeva izjava o skladnosti Kitajske
Slovenian
2024-06-19
NSYSPS3200 Dobaviteljeva izjava o skladnosti Kitajske
Stranska plošča podnožja Spacial SM - 200 x 300 mm
NSYSPS3200 Uredba REACH
Slovenian
2024-06-19
NSYSPS3200 Uredba REACH
Stranska plošča podnožja Spacial SM - 200 x 300 mm
CAD
Spacial SF-SM - Side panels plinth - H200xD300 mm - 3D CAD