This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
"This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU, with a change in range name going from Spacial SF to PanelSeT SFN. This version as well, provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view on the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased references"
In exposed environments, particular attention must be paid to the choice of enclosures. Stainless steel is the solution to resist aggression in exposed environments. This guide will help the reader to select the optimum stainless-steel enclosure accordingly.
CAE
Spacial S3D CAE package for EPLAN
SILENT
2024-04-15
Izjava o zaštiti životne sredine
PEP-Metallic Mounting plate
English
2024-04-15
Deklaracija usaglašenosti
NSYMF1010 EU RoHS deklaracija
Serbian
2024-04-02
NSYMF1010 EU RoHS deklaracija
mikroperforirana montažna ploča V1000xŠ1000 prečnik otvora 3,6mm na razm. 12,5mm
NSYMF1010 REACh deklaracija
Serbian
2024-04-02
NSYMF1010 REACh deklaracija
mikroperforirana montažna ploča V1000xŠ1000 prečnik otvora 3,6mm na razm. 12,5mm
NSYMF1010 RoHS deklaracija za Kinu
Serbian
2024-04-02
NSYMF1010 RoHS deklaracija za Kinu
mikroperforirana montažna ploča V1000xŠ1000 prečnik otvora 3,6mm na razm. 12,5mm
CAD
Spacial CRN - Microperf mount plate1000x1000 - 3D CAD