This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
"This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU, with a change in range name going from Spacial SF to PanelSeT SFN. This version as well, provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view on the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased references"
In exposed environments, particular attention must be paid to the choice of enclosures. Stainless steel is the solution to resist aggression in exposed environments. This guide will help the reader to select the optimum stainless-steel enclosure accordingly.
Izjava o zaštiti životne sredine
PEP-Metallic Mounting plate
English
2024-04-15
Deklaracija usaglašenosti
NSYMF32 EU RoHS deklaracija
Serbian
2024-04-02
NSYMF32 EU RoHS deklaracija
mikroperforirana montažna ploča V300xŠ200 prečnik otvora 3,6mm na razmaku 12,5mm
NSYMF32 REACh deklaracija
Serbian
2024-04-02
NSYMF32 REACh deklaracija
mikroperforirana montažna ploča V300xŠ200 prečnik otvora 3,6mm na razmaku 12,5mm
NSYMF32 RoHS deklaracija za Kinu
Serbian
2024-04-02
NSYMF32 RoHS deklaracija za Kinu
mikroperforirana montažna ploča V300xŠ200 prečnik otvora 3,6mm na razmaku 12,5mm
Uputstvo za upotrebu
instruction sheet for PLM32
SILENT
2024-04-15
CAD
Spacial S3D - NSYMF32 - Microperf mount plate 300x200