This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
Thalassa PLA Central Upright: How to Disassemble-Assemble
A fast and easy way to disassemble and assemble the central upright of the two-doors Thalassa PLA polyester floor-standing enclosures versions by maintaining the IP protection.Also allowing the installation of the mounting plate directly without any obstacles and reduce any possible damages to the devices installed on it.Applicable for two-doors Thalassa Heavy Duty enclosures version.