This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
Profil environnemental
PEP-Thalassa PLA
English
2024-06-15
Brochure
Brochure Thalassa - Enveloppes en polyester renforcé en fibre de verre
French
2024-06-15
Déclaration de conformité
NSYAEDPLA002G Déclaration REACh
French
2024-06-19
NSYAEDPLA002G Déclaration REACh
Thalassa - Jeu de 2 gâches pour armoire polyester PLA 2 portes Ral 7035
NSYAEDPLA002G Déclaration RoHS pour la Chine
French
2024-06-19
NSYAEDPLA002G Déclaration RoHS pour la Chine
Thalassa - Jeu de 2 gâches pour armoire polyester PLA 2 portes Ral 7035
NSYAEDPLA002G Déclaration RoHS UE
French
2024-06-19
NSYAEDPLA002G Déclaration RoHS UE
Thalassa - Jeu de 2 gâches pour armoire polyester PLA 2 portes Ral 7035