This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
This new version of the document takes into account the launch of the new offers. It also takes into account the change in range name from all Spacial offer to PanelSeT and all Thalassa TBS/TBP to PanelSeT TBS/TBP.
CAE
EPLAN_EDZ_Thalassa_PLA_package
SILENT
2024-06-30
Profil environnemental
PEP-Metallic Mounting plate
English
2024-06-15
Notice de montage
Thalassa PLA - PLAT - PLAZT - PLAZ - Notice de montage