This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
"This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU, with a change in range name going from Spacial SF to PanelSeT SFN. This version as well, provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view on the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased references"
Certificat
BVM_Certificate_Spacial-NSYSF-NSYSM ranges
English
2024-04-15
DoC
Russian
2024-04-15
TC_DEKRA_SPACIAL_SM
English
2024-04-15
TC_DEKRA_SPACIAL_SM
TC_DEKRA_SPACIAL_SM_ According to IEC62208
ЕАЭС_N_RU_Д-FR.PA01.B.80899_20
Russian
2024-04-15
Déclaration de conformité
Declaration of EU conformity for Spacial SM and Declaration of EU conformity for Spacial SM HF
English
2024-04-15
Profil environnemental
UE_Spacial SF, Steel floor-standing enclosure
English
2024-04-15
Déclaration de conformité
NSYSM2012502D Déclaration REACh
French
2024-04-17
NSYSM2012502D Déclaration REACh
Spacial SM - armoire monobloc - 2 portes - 2000x1200x500mm
NSYSM2012502D Déclaration RoHS pour la Chine
French
2024-04-17
NSYSM2012502D Déclaration RoHS pour la Chine
Spacial SM - armoire monobloc - 2 portes - 2000x1200x500mm
NSYSM2012502D Déclaration RoHS UE
French
2024-04-17
NSYSM2012502D Déclaration RoHS UE
Spacial SM - armoire monobloc - 2 portes - 2000x1200x500mm
CAE
Spacial SM CAE package for EPLAN
SILENT
2024-04-15
Spacial SM CAE package for EPLAN
This package contains 2D and 3D macros for ePlan, related to SM enclosures and their accessories