Communication Parameters Manual describes:
- The operating modes specific to communication (state chart)
- The interaction between communication and local control
- The control, reference, and monitoring parameters, with specific information for use via a bus or communication network It do not include the drive adjustment and configuration parameters, which are contained in the Excel file supplied as an appendix to this manual.
All the parameters are grouped together in an Excel file supplied as an appendix, with the following data:
- Code
- Name
- Addresses: logic, CANopen, INTERBUS, Device Net
- Category
- Read/write access
- Type: signed numerical, unsigned numerical, etc.
- Unit
- Factory setting
- Minimum value
- Maximum value
- Display on the graphic display terminal and the 7-segment integrated display terminal
- Relevant menu. This file offers the option of sorting and arranging the data according to any criterion chosen by the user.
ATV71 Communication parameters manuals
English
2024-06-15
ATV71 Communication parameters manuals
The pdf file describes the communication parameters. The Excel file provides the Fieldbus addresses
Instruction Sheet - migration table ATV71L to ATV LIFT
English
2024-06-15
Instruction Sheet: China RoHS - Hazardous Substances Table
Chinese,English
2024-06-19
Instruction Sheet: China RoHS - Hazardous Substances Table
This table is made according to SJ/T 11364. O: indicates that the concentration of a hazardous substance in all of the homogeneous materials for this part is below the limit as stipulated in GB/T 26572. X: indicates that the concentration of a hazardous substance in at least one of the homogeneous materials used for this part is above the limit as stipulated in GB/T 26572
Katalógus
Catalog: Altivar 71/71 Plus variable speed drives - English version 2014/04 (web pdf format)