This technical note outlines the compliance of applicable PowerLogic meters with the International Electrotechnical Commission’s IEC 61000-4-30 (or “4-30”) standard and is intended for personnel with knowledge of power quality and power quality standards.
ION Reference
English
2024-04-15
ION Reference
Overview of ION architecture and details of all ION modules
This document explains how to configure and operate ION9000 meters.
Upgrade PM89RD96 display firmware to v4.0.15
English
2024-04-15
Upgrade PM89RD96 display firmware to v4.0.15
This document describes the process to upgrade RD96 display firmware to the latest version for use with PowerLogic™ ION9000, PM8000 or ION7400 series meters.
What’s new for Power and Energy Monitoring Systems — November 2019
English
2024-04-15
What’s new for Power and Energy Monitoring Systems — November 2019
This update provides a summary of technological advances in the Power and Energy Monitoring System offers, and the technical documentation accompanying their release.
Firmware - Kiadott
ION9000 v4.0.0 Firmware and Associated Files
English
2024-04-15
ION9000 v4.0.0 Firmware and Associated Files
This ZIP file contains the files to upgrade the PowerLogic™ ION9000 series meter to firmware v4.0.0 (V004.000.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the upgrade section of the User Manual to perform this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the file. Name: ION9000_V004.000.000+200.zip Size: 43634681 bytes (41 MiB) SHA256: B71F0493170B8D23E50053FFC07DF096480BDA63CAC70AAF072DACF76CA64391
ION9000 v4.5.0 Firmware and Associated Files
English
2024-04-15
ION9000 v4.5.0 Firmware and Associated Files
This ZIP file contains the files to upgrade the PowerLogic™ ION9000 series meter to firmware v4.5.0 (V004.005.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the upgrade section of the User Manual to perform this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the file. ------------------------------------------Name: ION9000_V004.005.000+326.zip Size: 43861291 bytes (41 MiB) SHA256: 7b4b4603bde1cdc313817c9f80788366a470a9b213de7da7d754f1e9cc536182
Megfelelőségi nyilatkozat
DoC DE ION9000
Russian
2024-04-15
UK Declaration of Conformity
English
2024-04-15
UK Declaration of Conformity
UK Declaration of Conformity for the ION9000 series meter
Műszaki adatlap
PowerLogic ION9000 Technical Datasheet
English
2024-04-15
Tanúsítvány
PowerLogic ION9000 - NMi Certin B.V. - Type evaluation report