Important notice:SoMachine Configuration Manager must be update to the version 433.18.34401.0 before apply "SoMachine 4.1_TLS1.2_Add-on 4.1.0.0_21.07.30.1.seco" update file "SoMachineConfigurationManagerInstaller_433.18.34401.zip" is found in the seco package or can be downloaded from SE.COMDescription:The TLS 1.2 add-on is an update package for SoMachine V4.1.NOTE: TLS (Transport Layer Security) is used for secure data communication.This add-on introduces the update of the License Manager integration to enable the registration with the newest version of the License Server.
SoMachine 4.1 SP2 TLS 1.2 Add-on
English
2024-05-15
SoMachine 4.1 SP2 TLS 1.2 Add-on
Important notice:SoMachine Configuration Manager must be update to the version 433.18.34401.0 before apply "SoMV4.1_SP2_TLS1.2_AddOn_4.1.0.1_21.07.30.1.seco" update file "SoMachineConfigurationManagerInstaller_433.18.34401.zip" is found in the seco package or can be downloaded from SE.COMDescription:The TLS 1.2 add-on is an update package for SoMachine V4.1 SP2.NOTE: TLS (Transport Layer Security) is used for secure data communication.This add-on introduces the update of the License Manager integration to enable the registration with the newest version of the License Server.
SoMachine Motion 4.0 TLS 1.2 Add-on
English
2024-05-15
SoMachine Motion 4.0 TLS 1.2 Add-on
Important notice:SoMachine Configuration Manager must be update to the version 433.18.34401.0 before apply "SoMMV4.0_TLS1.2_AddOn_4.0.0.0_21.07.30.1.seco" update file "SoMachineConfigurationManagerInstaller_433.18.34401.zip" is found in the seco package or can be downloaded from SE.COMDescription:The TLS 1.2 add-on is an update package for SoMachine Motion V4.0.NOTE: TLS (Transport Layer Security) is used for secure data communication.This add-on introduces the update of the License Manager integration to enable the registration with the newest version of the License Server.
SoMachine Motion 4.1 TLS 1.2 Add-on
English
2024-05-15
SoMachine Motion 4.1 TLS 1.2 Add-on
The TLS 1.2 add-on is an update package for SoMachine Motion V4.1.NOTE: TLS (Transport Layer Security) is used for secure data communication.This add-on introduces the update of the License Manager integration to enable the registration with the newest version of the License Server.
SoMachine Motion 4.2 TLS 1.2 Add-on
English
2024-05-15
SoMachine Motion 4.2 TLS 1.2 Add-on
The TLS 1.2 add-on is an update package for SoMachine Motion V4.2.NOTE: TLS (Transport Layer Security) is used for secure data communication.This add-on introduces the update of the License Manager integration to enable the registration with the newest version of the License Server.
SoMachine Configuration Manager Version 433.18.34401
This installer introduces the update of the License Manager integration to enable the registration with the newest version of the License Server.
This version is needed to be installed before introducing following new SECO files for SoMachine Motion V4.0 and V4.1 and SoMachine V4.1
Related SECO files:
SoMMV4.0_TLS1.2_AddOn_4.0.0.0_21.07.30.1.seco
SoMMV4.1_TLS1.2_AddOn_4.1.0.0_21.07.30.1.seco
SoMMV4.2_TLS1.2_AddOn_4.2.0.0_21.07.30.1.seco
SoMV4.1_TLS1.2_AddOn_4.1.0.0_21.07.30.1.seco
SoMV4.1_SP2_TLS1.2_AddOn_4.1.0.1_21.07.30.1.seco