This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
CAE
Spacial CRN CAE package for EPLAN
SILENT
2024-06-20
Certificat
DoC
Russian
2024-06-19
ЕАЭС_N_RU_Д-FR.PA01.B.80899_20
Russian
2024-06-19
Сертификат оболочки (шкафы) пустые для низковольтных комплектных устройств серии Spacial S3D и серии Spacial CRN
Russian
2024-06-20
Сертификат шкафы из стали и промышленные коробки серии Spacial