Schneider-Electric
 
AF1VA416 image- Schneider-electric
AF1VA416
PanelSeT - Thalassa - VIS H 4X16 A RONDELLE
Statut commercial Statut commercial: 
Commercialisé
Schneider Electric
Téléchargements et Documents 1 à 5 sur 5
Catalogue
 
Catalogue Enveloppes universelles French   2024-07-15  summary
Catalogue Enveloppes universelles

Boîtes industrielles acier Coffrets acier Armoires et cellules acier Coffrets inox Armoires et cellules inox Boîtes isolantes Coffrets isolants Armoires isolantes Accessoires Solutions applicatives et personnalisées Gestion thermique Guides techniques et pièces détachées
 
Universal Enclosures - 2023 Catalog (English) English   2024-07-17  summary
Universal Enclosures - 2023 Catalog (English)

This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
 
 
Déclaration de conformité
 
AF1VA416 Déclaration REACh French   2024-07-06  summary
AF1VA416 Déclaration REACh

VIS H 4X16 A RONDELLE
 
AF1VA416 Déclaration RoHS pour la Chine French   2024-07-06  summary
AF1VA416 Déclaration RoHS pour la Chine

VIS H 4X16 A RONDELLE
 
AF1VA416 Déclaration RoHS UE French   2024-07-06  summary
AF1VA416 Déclaration RoHS UE

VIS H 4X16 A RONDELLE