This technical note outlines the compliance of applicable PowerLogic meters with the International Electrotechnical Commission’s IEC 61000-4-30 (or “4-30”) standard and is intended for personnel with knowledge of power quality and power quality standards.
Instructions on how to install, configure, use, and maintain PowerLogic PM8000 series devices.
PowerLogic PM8000 series User Manual DE
German,English
2024-06-15
PowerLogic PM8000 series User Manual DE
How to install, configure, use, and maintain a PM8000 series device.
PowerLogic Серия PM8000 Руководство пользователя
Russian
2024-06-15
Upgrade meter firmware to v2.2.1
English
2024-06-15
Upgrade meter firmware to v2.2.1
This document describes the process to upgrade PowerLogic™ ION9000, PM8000 or ION7400 series meters to the latest firmware version. It also contains information about upgrading analog I/O option module firmware.
Upgrade PM89RD96 display firmware to v4.0.15
English
2024-06-15
Upgrade PM89RD96 display firmware to v4.0.15
This document describes the process to upgrade RD96 display firmware to the latest version for use with PowerLogic™ ION9000, PM8000 or ION7400 series meters.
What’s new for Power and Energy Monitoring Systems — November 2019
English
2024-06-15
What’s new for Power and Energy Monitoring Systems — November 2019
This update provides a summary of technological advances in the Power and Energy Monitoring System offers, and the technical documentation accompanying their release.
What’s new in PM8000 series firmware v1.3.1
English
2024-06-15
What’s new in PM8000 series firmware v1.3.1
Firmware version v1.3.1 for the PM8000 series meter adds Internal clock temperature compensation feature and resolves previously unknown Modbus master issue. This document also contains IPv6 global addressing and IPv6 gateway support content from the previous what's new document (7EN12-0295).
What’s new in PM8000 series firmware v1.4.1
English
2024-06-15
What’s new in PM8000 series firmware v1.4.1
Firmware version v1.4.1 for the PM8000 series meter adds security enhancements, new communications functionality, increased onboard log storage capacity, a webpage waveform viewer and other improvements.
What’s new in PM8000 series meter firmware v2.1.0
English
2024-06-15
What’s new in PM8000 series meter firmware v2.1.0
Whats New in PM8000 v2.1.0 firmware. The following new features are included:
Enhanced firmware upgrades,
PTP time synchronization,
Secure webserver (HTTPS),
other
Firmware
METSEPM89M0024 Analog I/O Module V001.002.000 firmware
English
2024-05-15
METSEPM89M0024 Analog I/O Module V001.002.000 firmware
The 1.2.0 (V001.002.000) firmware for the METSEPM89M0024 Analog I/O Module adds 0-20 mA support when used with PM8000, ION7400, or ION9000 meter firmware 2.1.0 (V002.001.000) or higher. SHA256 File signatures:77855de93e70ed9b25be9568b64eaa333c56ead286624323fbc04073cdb5626a *METSEPM89M0024_AIO_V001.002.000_Release.s19
METSEPM89M2600 Digital I/O Module V001.002.000 firmware
English
2024-06-15
METSEPM89M2600 Digital I/O Module V001.002.000 firmware
The 1.2.0 (V001.002.000) firmware for the METSEPM89M2600 Digital I/O Module is compatible with PM8000, ION7400, and ION9000 meters. SHA256 File signatures: 5f88067ed29ef9d7c369410fb1785967cf1838436062a0509c6aee1ad7f0c412 *METSEPM89M2600_DIO_V001.002.000_Release.s19
PM8000 V002.001.000 (v 2.1.0) Firmware and Associated Files (Meter Template, Modbus Map document, SNMP MIB, Web pages)
English
2024-06-15
PM8000 V002.001.000 (v 2.1.0) Firmware and Associated Files (Meter Template, Modbus Map document, SNMP MIB, Web pages)
Firmware version 2.1.0 for the PowerLogic™ PM8000 series meter adds enhanced firmware upgrade support, PTP, Secure HTTPS webserver, ION Module updates, updated support for the latest versions of EN50160, IEEE 519 and IEC 61000-4-30 power quality standards, pre- and post-event data capture for data and waveform recorders, and 0-20 mA support for the Analog I/O option module.To upgrade your meter to firmware version 2.1.0, you must use ION Setup version 3.1 or later. Please refer to the “Upgrading devices to firmware v2.1.0” technical note at https://www.schneider-electric.com/en/download/document/7EN72-0203/ for instructions on upgrading your meter firmware to version 2.1.0.SHA256 File signatures:3cdd6e69bfa85d8b76255391270db77f504ec77385bd2dfbc3c7f6b62f31c097 *PM8000_V002.001.000.zip
PM8000 v3.0.0 Firmware and Associated Files
English
2024-06-15
PM8000 v3.0.0 Firmware and Associated Files
'This ZIP file contains the files to upgrade the PowerLogic™ PM8000 series meter to firmware v3.0.0 (V003.000.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the Upgrading Meter Firmware to v3.0.0 document for important information on performing this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the PM8000_V003.000.000+599.zip file.Name: PM8000_V003.000.000+599.zipSHA256: F54D8348FE77242A88878F946DD9527109D850CC8A6CEF6AA4F3FDDC96971BA1
PM8000 v3.1.0 Firmware and Associated Files
English
2024-06-15
PM8000 v3.1.0 Firmware and Associated Files
'This ZIP file contains the files to upgrade the PowerLogic™ PM8000 series meter to firmware v3.1.0 (V003.001.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the upgrade section of the User Manual to perform this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the file. Name: PM8000_V003.001.000+626.zip SHA256: 073C0192EE8A0B833F273AB7D65E7E51AD1C813590CE5CB56D859394F5A8EC6A
PM8000 v4.0.0 Firmware and Associated Files
English
2024-06-15
PM8000 v4.0.0 Firmware and Associated Files
This ZIP file contains the files to upgrade the PowerLogic™ PM8000 series meter to firmware v4.0.0 (V004.000.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the upgrade section of the User Manual to perform this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the file. Name: PM8000_V004.000.000+200.zip Size: 19341150 bytes (18 MiB) SHA256: D97EC88AF4937B2522120FF3836EA7316CFC87291575EAFAAF8E674D07DB41C5
PM8000 v4.5.0 Firmware and Associated Files
English
2024-06-15
PM8000 v4.5.0 Firmware and Associated Files
This ZIP file contains the files to upgrade the PowerLogic™ PM8000 series meter to firmware v4.5.0 (V004.005.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the upgrade section of the User Manual to perform this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the file. ----------------------------------------- Name: PM8000_V004.005.000+326.zip Size: 19933157 bytes (19 MiB) SHA256: a320e0e93a4b96d4edcea16f6dff84aa44f81e1ee595e58ed48abbb59fc792f1
PowerLogic PM89RD96 Display OS Package Firmware version 4.0.0 - supports v2.0.0 meter firmware
English
2024-06-15
PowerLogic PM89RD96 Display OS Package Firmware version 4.0.0 - supports v2.0.0 meter firmware
This is OS Package version 4.0.0 for the METSEPM89RD96 remote display. It supports meter firmware version 2.0.0, including the PowerLogic™ ION9000 series.See the Power Meter user manual for display firmware upgrade instructions.Note: This remote display OS Package is not compatible with PM8000 & ION7400 meters running firmware versions 1.4.x and older.SHA256 File signatures:8b0aaa760d1e705b7528ee3941e381c00cab3adc524b460a9fd04acf54a0ef37 *rmdupg_rd96_004.000.000.bin
Software - Release
What's new in PowerLogic PM8000 series meter firmware v4.5.0
English
2024-06-15
What's new in PowerLogic PM8000 series meter firmware v4.5.0
Summary of the new features included in firmware version 4.5.0
What's new in PowerLogic™ PM8000 series meter firmware v3.1.0
English
2024-06-15
What's new in PowerLogic™ PM8000 series meter firmware v3.1.0
Summary of the new features included in firmware version 3.1.0
The installation guide for PowerLogic PM8243 power and energy DIN-mount meter describes mounting, wiring, connecting and verifying operation of the meter.
Installation instructions for the digital I/O option module
Other technical guide
PowerLogic PM8000 Technical Datasheet
English
2024-06-15
Catalogue
PowerLogic Power Monitoring and Control Catalog - Web
English
2024-06-19
PowerLogic Power Monitoring and Control Catalog - Web
PowerLogic Products Catalogue. Note that no printed catalogues are available but all necessary source files in 13 sections are available for download from the Shopping Kiosk.
Known issues: PM8000 series firmware version v1.2.14 and v1.2.15
English
2024-06-15
Known issues: PM8000 series firmware version v1.2.14 and v1.2.15
After upgrading your PM8000 series meter to firmware version v1.2.14 or v1.2.15, pasting a custom framework onto the meter causes the Summary screen to display a blank screen after the menu button is pressed.
Circularity Profile
PowerLogic PM8000 PM8244, Circularity Profile, End of Life Instructions
English
2024-06-15
Environmental disclosure
PowerLogic PM8000 PM8243 DIN rail mount meter, Environmental Disclosure, Product Environmental Profile
English
2024-06-15
CAD
PM8000 DIN Rail Mount Meter 3D - Simplified - 3D CAD