Instructions on how to install, configure, use, and maintain PowerLogic PM8000 series devices.
PowerLogic PM8000 series User Manual DE
German,English
2024-06-15
PowerLogic PM8000 series User Manual DE
How to install, configure, use, and maintain a PM8000 series device.
PowerLogic Серия PM8000 Руководство пользователя
Russian
2024-06-15
Upgrade meter firmware to v2.2.1
English
2024-06-15
Upgrade meter firmware to v2.2.1
This document describes the process to upgrade PowerLogic™ ION9000, PM8000 or ION7400 series meters to the latest firmware version. It also contains information about upgrading analog I/O option module firmware.
What’s new in ION9000 series meter firmware v2.1.0
English
2024-05-15
What’s new in ION9000 series meter firmware v2.1.0
ION9000 firmware version 2.1.0 updates: 0-20 mA Analog I/O option module support, UPG to UPX firmware upgrade enhancement
What’s new in PM8000 series meter firmware v2.1.0
English
2024-06-15
What’s new in PM8000 series meter firmware v2.1.0
Whats New in PM8000 v2.1.0 firmware. The following new features are included:
Enhanced firmware upgrades,
PTP time synchronization,
Secure webserver (HTTPS),
other
Firmware
METSEPM89M0024 Analog I/O Module V001.002.000 firmware
English
2024-05-15
METSEPM89M0024 Analog I/O Module V001.002.000 firmware
The 1.2.0 (V001.002.000) firmware for the METSEPM89M0024 Analog I/O Module adds 0-20 mA support when used with PM8000, ION7400, or ION9000 meter firmware 2.1.0 (V002.001.000) or higher. SHA256 File signatures:77855de93e70ed9b25be9568b64eaa333c56ead286624323fbc04073cdb5626a *METSEPM89M0024_AIO_V001.002.000_Release.s19
METSEPM89M2600 Digital I/O Module V001.002.000 firmware
English
2024-06-15
METSEPM89M2600 Digital I/O Module V001.002.000 firmware
The 1.2.0 (V001.002.000) firmware for the METSEPM89M2600 Digital I/O Module is compatible with PM8000, ION7400, and ION9000 meters. SHA256 File signatures: 5f88067ed29ef9d7c369410fb1785967cf1838436062a0509c6aee1ad7f0c412 *METSEPM89M2600_DIO_V001.002.000_Release.s19
PM8000 V002.001.000 (v 2.1.0) Firmware and Associated Files (Meter Template, Modbus Map document, SNMP MIB, Web pages)
English
2024-06-15
PM8000 V002.001.000 (v 2.1.0) Firmware and Associated Files (Meter Template, Modbus Map document, SNMP MIB, Web pages)
Firmware version 2.1.0 for the PowerLogic™ PM8000 series meter adds enhanced firmware upgrade support, PTP, Secure HTTPS webserver, ION Module updates, updated support for the latest versions of EN50160, IEEE 519 and IEC 61000-4-30 power quality standards, pre- and post-event data capture for data and waveform recorders, and 0-20 mA support for the Analog I/O option module.To upgrade your meter to firmware version 2.1.0, you must use ION Setup version 3.1 or later. Please refer to the “Upgrading devices to firmware v2.1.0” technical note at https://www.schneider-electric.com/en/download/document/7EN72-0203/ for instructions on upgrading your meter firmware to version 2.1.0.SHA256 File signatures:3cdd6e69bfa85d8b76255391270db77f504ec77385bd2dfbc3c7f6b62f31c097 *PM8000_V002.001.000.zip
PM8000 v3.0.0 Firmware and Associated Files
English
2024-06-15
PM8000 v3.0.0 Firmware and Associated Files
'This ZIP file contains the files to upgrade the PowerLogic™ PM8000 series meter to firmware v3.0.0 (V003.000.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the Upgrading Meter Firmware to v3.0.0 document for important information on performing this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the PM8000_V003.000.000+599.zip file.Name: PM8000_V003.000.000+599.zipSHA256: F54D8348FE77242A88878F946DD9527109D850CC8A6CEF6AA4F3FDDC96971BA1
PM8000 v3.1.0 Firmware and Associated Files
English
2024-06-15
PM8000 v3.1.0 Firmware and Associated Files
'This ZIP file contains the files to upgrade the PowerLogic™ PM8000 series meter to firmware v3.1.0 (V003.001.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the upgrade section of the User Manual to perform this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the file. Name: PM8000_V003.001.000+626.zip SHA256: 073C0192EE8A0B833F273AB7D65E7E51AD1C813590CE5CB56D859394F5A8EC6A
PM8000 v4.0.0 Firmware and Associated Files
English
2024-06-15
PM8000 v4.0.0 Firmware and Associated Files
This ZIP file contains the files to upgrade the PowerLogic™ PM8000 series meter to firmware v4.0.0 (V004.000.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the upgrade section of the User Manual to perform this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the file. Name: PM8000_V004.000.000+200.zip Size: 19341150 bytes (18 MiB) SHA256: D97EC88AF4937B2522120FF3836EA7316CFC87291575EAFAAF8E674D07DB41C5
PM8000 v4.5.0 Firmware and Associated Files
English
2024-06-15
PM8000 v4.5.0 Firmware and Associated Files
This ZIP file contains the files to upgrade the PowerLogic™ PM8000 series meter to firmware v4.5.0 (V004.005.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the upgrade section of the User Manual to perform this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the file. ----------------------------------------- Name: PM8000_V004.005.000+326.zip Size: 19933157 bytes (19 MiB) SHA256: a320e0e93a4b96d4edcea16f6dff84aa44f81e1ee595e58ed48abbb59fc792f1
PowerLogic PM89RD96 Display OS Package Firmware version 4.0.0 - supports v2.0.0 meter firmware
English
2024-06-15
PowerLogic PM89RD96 Display OS Package Firmware version 4.0.0 - supports v2.0.0 meter firmware
This is OS Package version 4.0.0 for the METSEPM89RD96 remote display. It supports meter firmware version 2.0.0, including the PowerLogic™ ION9000 series.See the Power Meter user manual for display firmware upgrade instructions.Note: This remote display OS Package is not compatible with PM8000 & ION7400 meters running firmware versions 1.4.x and older.SHA256 File signatures:8b0aaa760d1e705b7528ee3941e381c00cab3adc524b460a9fd04acf54a0ef37 *rmdupg_rd96_004.000.000.bin
Software - Release
What's new in PowerLogic PM8000 series meter firmware v4.5.0
English
2024-06-15
What's new in PowerLogic PM8000 series meter firmware v4.5.0
Summary of the new features included in firmware version 4.5.0
What's new in PowerLogic™ PM8000 series meter firmware v3.1.0
English
2024-06-15
What's new in PowerLogic™ PM8000 series meter firmware v3.1.0
Summary of the new features included in firmware version 3.1.0
Catalogue
PowerLogic Power Monitoring and Control Catalog - Web
English
2024-06-19
PowerLogic Power Monitoring and Control Catalog - Web
PowerLogic Products Catalogue. Note that no printed catalogues are available but all necessary source files in 13 sections are available for download from the Shopping Kiosk.