This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
This new version of the document takes into account the launch of the new offers. It also takes into account the change in range name from all Spacial offer to PanelSeT and all Thalassa TBS/TBP to PanelSeT TBS/TBP.
Environmental disclosure
UE_Spacial SF, Steel floor-standing enclosure
English
2024-06-15
Declaration of conformity
NSYSPS3200 China RoHS Declaration
English
2024-06-27
NSYSPS3200 China RoHS Declaration
Spacial SM side panel plinth - 200x300 mm
NSYSPS3200 EU RoHS Declaration
English
2024-06-27
NSYSPS3200 EU RoHS Declaration
Spacial SM side panel plinth - 200x300 mm
NSYSPS3200 REACh Declaration
English
2024-06-27
NSYSPS3200 REACh Declaration
Spacial SM side panel plinth - 200x300 mm
CAD
Spacial SF-SM - Side panels plinth - H200xD300 mm - 3D CAD