The attached zip file contains the following files: (1) PM5560_PM5563_Maintenance_Upgrades_v2.0.1.pdf (2) PM5560_PM5563_PublicFirmwareRevisionHistory_v2.0.1.pdf (3) PM5560_PM5563_PublicModbusRegisterList_v2.0.1.xlsx (4) PM5560_PM5563_WhatsNew_v2.0.1.pdf (5) PM556x_v2.0.1.fwa (6) App2.out (7) PM5500StartUpgrade.shtmlNOTE: There is a new method for upgrading the firmware on your meter and its Ethernet communications system. The new method simply uses FTP to copy files from your computer to the meter’s FTP server. The FTP server is accessed using the same login credentials as the meter webpages. Detailed instructions for how to upgrade the meter using this new technique are found in PM5560_PM5563_Maintenance_Upgrades_v2.0.1.pdf.IMPORTANT: For MID compliance, the PM5561 meter’s firmware upgrade functionality is permanently disabled. Thus this firmware upgrade applies only to the PM5560 and PM5563.
The DNP3 protocol support over Ethernet is available in firmware version 2.7.4 and above for PM5560, PM5563, and PM5563RD meter models. The Distributed Network Protocol Version 3.0 (DNP3) is a multipoint communication protocol that specifies the coding of data and rules for exchanging data between a slave device and a master control device. DNP3 is an open protocol that can be implemented on any communication device. The DNP3 is available on Ethernet communication.
PowerLogic Energy & Power Meters Catalogue for Panel Builders
English
2024-06-19
PowerLogic Power Monitoring and Control Catalog - Web
English
2024-06-19
PowerLogic Power Monitoring and Control Catalog - Web
PowerLogic Products Catalogue. Note that no printed catalogues are available but all necessary source files in 13 sections are available for download from the Shopping Kiosk.
Anden teknisk vejledning
PowerLogic PM5000 Series Technical Datasheet
English
2024-06-15
Technical illustration
Illustration: Dimensions Drawing for PM5563
English
2024-06-15
Overensstemmelseserklæring
METSEPM5563 REACh-erklæring
Danish
2024-06-25
METSEPM5563 REACh-erklæring
PM5563 strømmåler uden display - op til 63th H - 4DI/2DO 52 alarmer
METSEPM5563 RoHS-erklæring for EUR
Danish
2024-06-25
METSEPM5563 RoHS-erklæring for EUR
PM5563 strømmåler uden display - op til 63th H - 4DI/2DO 52 alarmer
METSEPM5563 RoHS-erklæring for Kina
Danish
2024-06-25
METSEPM5563 RoHS-erklæring for Kina
PM5563 strømmåler uden display - op til 63th H - 4DI/2DO 52 alarmer
Software - Hotfix
PM5500/5600/5700 Series SE Driver for PME 2020 (ENG)
English
2024-06-15
PM5500/5600/5700 Series SE Driver for PME 2020 (ENG)
Supports waveforms and PQ reportsSHA256 Hash Key : 9F9C1B630AFE32C69BBCB4E0C26A427771991512C878FC22ABE38076D748E7A0
PM5500/5600/5700 Series SE Driver for PME 9.0 (ENG)
English
2024-06-15
PM5500/5600/5700 Series SE Driver for PME 9.0 (ENG)
Supports waveforms and PQ reportsSHA256 Hash Key : BD9EF6B494A3BC9DC4B4528191EFD28A557264DE722E0FD6BC1A0890C11DEAEA
Cirkularitetsprofil
PowerLogic PM5563 Transducer Meter, Circularity Profile, End of Life Instructions