Instructions on how to install, configure, use, and maintain PowerLogic PM8000 series devices.
PowerLogic PM8000 series User Manual DE
German,English
2024-06-15
PowerLogic PM8000 series User Manual DE
How to install, configure, use, and maintain a PM8000 series device.
What’s new for Power and Energy Monitoring Systems — November 2019
English
2024-06-15
What’s new for Power and Energy Monitoring Systems — November 2019
This update provides a summary of technological advances in the Power and Energy Monitoring System offers, and the technical documentation accompanying their release.
What’s new in PM8000 series meter firmware v2.1.0
English
2024-06-15
What’s new in PM8000 series meter firmware v2.1.0
Whats New in PM8000 v2.1.0 firmware. The following new features are included:
Enhanced firmware upgrades,
PTP time synchronization,
Secure webserver (HTTPS),
other
Firmware
METSEPM89M0024 Analog I/O Module V001.002.000 firmware
English
2024-05-15
METSEPM89M0024 Analog I/O Module V001.002.000 firmware
The 1.2.0 (V001.002.000) firmware for the METSEPM89M0024 Analog I/O Module adds 0-20 mA support when used with PM8000, ION7400, or ION9000 meter firmware 2.1.0 (V002.001.000) or higher. SHA256 File signatures:77855de93e70ed9b25be9568b64eaa333c56ead286624323fbc04073cdb5626a *METSEPM89M0024_AIO_V001.002.000_Release.s19
PM8000 v3.1.0 Firmware and Associated Files
English
2024-06-15
PM8000 v3.1.0 Firmware and Associated Files
'This ZIP file contains the files to upgrade the PowerLogic™ PM8000 series meter to firmware v3.1.0 (V003.001.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the upgrade section of the User Manual to perform this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the file. Name: PM8000_V003.001.000+626.zip SHA256: 073C0192EE8A0B833F273AB7D65E7E51AD1C813590CE5CB56D859394F5A8EC6A
PM8000 v4.5.0 Firmware and Associated Files
English
2024-06-15
PM8000 v4.5.0 Firmware and Associated Files
This ZIP file contains the files to upgrade the PowerLogic™ PM8000 series meter to firmware v4.5.0 (V004.005.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the upgrade section of the User Manual to perform this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the file. ----------------------------------------- Name: PM8000_V004.005.000+326.zip Size: 19933157 bytes (19 MiB) SHA256: a320e0e93a4b96d4edcea16f6dff84aa44f81e1ee595e58ed48abbb59fc792f1
PowerLogic PM89RD96 Display OS Package Firmware version 4.0.0 - supports v2.0.0 meter firmware
English
2024-06-15
PowerLogic PM89RD96 Display OS Package Firmware version 4.0.0 - supports v2.0.0 meter firmware
This is OS Package version 4.0.0 for the METSEPM89RD96 remote display. It supports meter firmware version 2.0.0, including the PowerLogic™ ION9000 series.See the Power Meter user manual for display firmware upgrade instructions.Note: This remote display OS Package is not compatible with PM8000 & ION7400 meters running firmware versions 1.4.x and older.SHA256 File signatures:8b0aaa760d1e705b7528ee3941e381c00cab3adc524b460a9fd04acf54a0ef37 *rmdupg_rd96_004.000.000.bin
Installation sheet for PowerLogic PM8210 / PM8240 / PM8280 / PM82403 / PM82404 power and energy meters describes mounting, wiring, connecting and verifying operation of the meter.