Instructions on how to install, configure, use, and maintain PowerLogic PM8000 series devices.
PowerLogic PM8000 series User Manual DE
German,English
2024-06-15
PowerLogic PM8000 series User Manual DE
How to install, configure, use, and maintain a PM8000 series device.
Upgrade meter firmware to v2.2.1
English
2024-06-15
Upgrade meter firmware to v2.2.1
This document describes the process to upgrade PowerLogic™ ION9000, PM8000 or ION7400 series meters to the latest firmware version. It also contains information about upgrading analog I/O option module firmware.
Software - nye releases
What's new in PowerLogic PM8000 series meter firmware v4.5.0
English
2024-06-15
What's new in PowerLogic PM8000 series meter firmware v4.5.0
Summary of the new features included in firmware version 4.5.0
Anden teknisk vejledning
PowerLogic PM8000 Technical Datasheet
English
2024-06-15
Firmware
METSEPM89M0024 Analog I/O Module V001.002.000 firmware
English
2024-05-15
METSEPM89M0024 Analog I/O Module V001.002.000 firmware
The 1.2.0 (V001.002.000) firmware for the METSEPM89M0024 Analog I/O Module adds 0-20 mA support when used with PM8000, ION7400, or ION9000 meter firmware 2.1.0 (V002.001.000) or higher. SHA256 File signatures:77855de93e70ed9b25be9568b64eaa333c56ead286624323fbc04073cdb5626a *METSEPM89M0024_AIO_V001.002.000_Release.s19
PM8000 V002.001.000 (v 2.1.0) Firmware and Associated Files (Meter Template, Modbus Map document, SNMP MIB, Web pages)
English
2024-06-15
PM8000 V002.001.000 (v 2.1.0) Firmware and Associated Files (Meter Template, Modbus Map document, SNMP MIB, Web pages)
Firmware version 2.1.0 for the PowerLogic™ PM8000 series meter adds enhanced firmware upgrade support, PTP, Secure HTTPS webserver, ION Module updates, updated support for the latest versions of EN50160, IEEE 519 and IEC 61000-4-30 power quality standards, pre- and post-event data capture for data and waveform recorders, and 0-20 mA support for the Analog I/O option module.To upgrade your meter to firmware version 2.1.0, you must use ION Setup version 3.1 or later. Please refer to the “Upgrading devices to firmware v2.1.0” technical note at https://www.schneider-electric.com/en/download/document/7EN72-0203/ for instructions on upgrading your meter firmware to version 2.1.0.SHA256 File signatures:3cdd6e69bfa85d8b76255391270db77f504ec77385bd2dfbc3c7f6b62f31c097 *PM8000_V002.001.000.zip
PM8000 v3.0.0 Firmware and Associated Files
English
2024-06-15
PM8000 v3.0.0 Firmware and Associated Files
'This ZIP file contains the files to upgrade the PowerLogic™ PM8000 series meter to firmware v3.0.0 (V003.000.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the Upgrading Meter Firmware to v3.0.0 document for important information on performing this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the PM8000_V003.000.000+599.zip file.Name: PM8000_V003.000.000+599.zipSHA256: F54D8348FE77242A88878F946DD9527109D850CC8A6CEF6AA4F3FDDC96971BA1
PM8000 v3.1.0 Firmware and Associated Files
English
2024-06-15
PM8000 v3.1.0 Firmware and Associated Files
'This ZIP file contains the files to upgrade the PowerLogic™ PM8000 series meter to firmware v3.1.0 (V003.001.000), Meter Template, Modbus Map document, SNMP MIB, Webpages, What’s new document, and other associated files. See the upgrade section of the User Manual to perform this upgrade. Verify the checksum of the file to help ensure it was not corrupted during download using the SHA-256 File Signature for the file. Name: PM8000_V003.001.000+626.zip SHA256: 073C0192EE8A0B833F273AB7D65E7E51AD1C813590CE5CB56D859394F5A8EC6A
PowerLogic PM89RD96 Display OS Package Firmware version 4.0.0 - supports v2.0.0 meter firmware
English
2024-06-15
PowerLogic PM89RD96 Display OS Package Firmware version 4.0.0 - supports v2.0.0 meter firmware
This is OS Package version 4.0.0 for the METSEPM89RD96 remote display. It supports meter firmware version 2.0.0, including the PowerLogic™ ION9000 series.See the Power Meter user manual for display firmware upgrade instructions.Note: This remote display OS Package is not compatible with PM8000 & ION7400 meters running firmware versions 1.4.x and older.SHA256 File signatures:8b0aaa760d1e705b7528ee3941e381c00cab3adc524b460a9fd04acf54a0ef37 *rmdupg_rd96_004.000.000.bin