This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
This new version of the document takes into account the launch of the new offers. It also takes into account the change in range name from all Spacial offer to PanelSeT and all Thalassa TBS/TBP to PanelSeT TBS/TBP.
Instruktionsark
PanelSeT SFN (Assembled Supply) and Main Accessories – Instruction Sheet
Introducing PanelSeTSFN & ConnectedCoolingUnit - eco-friendly solutions to protect your solutions and devices. Discover this revolutionary duo that reduces carbon footprint while ensuring utmost safety. An amazing combo!
CAE
PanelSeT SFN & PrismaSeT HD complete range CAE package for EPLAN
PanelSeT SFN – How to use the coupling kit | Schneider Electric Support
The Spacial SFN´s coupling kit composed by steel flat connectors, brackets and an EPDM gasket is the perfect solution for joining enclosures side-to-side or depthwide providing a strong and secure connection.
Spacial SFN - How to Install and couple plinths | Schneider Electric
The Spacial SFN plinth is a robust and stable base made of sheet steel finished with an epoxy polyester powder (RAL7022) that enables cable protection and management while ensuring a secure fixation between the enclosure and the floor, along with a slight elevation. Its design helps guarantee a dependable foundation for equipment, facilitating optimal performance, easy maintenance, and convenient access.The plinth comprises two components: the front and rear kit, which is determined by the enclosure's width, and the side panels, which determine the enclosure's depth. The number of side panels required varies depending on the specific plinth combination. There are different ways to couple the plinths and to fix it to the enclosure. Also compatible with Spacial SM compact floor standing enclosures.
Technical illustration
PanelSeT SFN Door Hinges - Product Installation
SILENT
2024-06-19
PanelSeT SFN Enclosure with plinth - Exploded view
SILENT
2024-06-19
PanelSeT SFN Manipulating the handle - Product Installation
SILENT
2024-06-22
PanelSeT SFN Plain door SFN 2000x400 - Image with Dimensions